Tool/software: Code Composer Studio
Hi fellows,
An amazing behavior happens in my CCS project.
When the code is loaded and launched by the JTAG debugger with the "Continous Refresh" function checked, the inputs are tacken into account, but very slowly (I mean in seconds).
But I unchecked this function during the run, the code does not react to inputs. The behavior is the same if the code is self-launched from power-up.
I would be very grateful if anyone could suggest any idea to understand this amazing behavior.
Regards.
HW :
CCS V8.3.1
JTAG : TMS320-XDS100V3+
DSC : TMDSCNCD28335