Part Number: CCSTUDIO-C2000
Hello,
I am using the CCS V10.1.1 command line interface. The commands are working, but I do not get any output in cmd window.
I can redirect the output by 1>outfile.txt, but not in cmd directly. E.g.
ccstudio -noSplash -data "D:\workspace" -application com.ti.ccstudio.apps.projectBuild -ccs.help
returns with no output. Calling this
ccstudio -noSplash -data "D:\workspace" -application com.ti.ccstudio.apps.projectBuild -ccs.help 1> help.txt 2>&1
help.txt contains the help output.
I used windows cmd and power shell, no success. Does anybody has an idea thats wrong?
Thanks Steffen