Part Number: CODECOMPOSER
Hello all,
According to the document "SPRA958L – January 2013 Running an Application from Internal Flash Memory on the TMS320F28xxx DSP": The hex utility should generate a .hex file with some starting hex for the bootloader (which includes the entry point), followed by the code to go into flash. When I put in an entrypoint of 0x3f123456 (Command line options --entrypoint=0x3f123456 --boot --ascii) I get the following first couple lines in the hex output:
AA 00 00 00 00 00 00 00 00 12 56 1A 3E 48 FF 00 00 01 FE 02 00 00 00 FE
04 00 00 00 FE 06 00 1D 3E FE 08 00 1D 3E 00 00
only the 12 and 56 from the entry point made it to the hex output.
If i put 0x3ff4fa, I get the following:
AA 00 00 00 00 00 00 00 00 3F FA 1A 3E 48 FF 00 00 01 FE 02 00 00 00 FE
04 00 00 00 FE 06 00 1D 3E FE 08 00 1D 3E 00 00
Again, missing some bytes for the entry point.
Whats going on here?