Other Parts Discussed in Thread: TIDM-DC-DC-BUCK, SFRA, C2000WARE
Hi,
I reference to the documtent
Reference Designs: TIDM-DC-DC-BUCK
C2000 Digital Power BoosterPack
Until 4.g everything is fine.
but with
Set BUCK_activeLoadContEnable to 1
I see still have a step which is not there. The output current is constant. The output voltage is constant.
from sample 300 i can see noise on the signal that I expect all the time from the beginning.
and when I start SFRA I see on the high level the sinus, but why is it up to 300sample low?
I expect something like
-Andreas