Other Parts Discussed in Thread: LAUNCHXL-F28027F
Hello, the development board I use is LAUNCHXL-F28027F + BOOSTXL-DRV83. The development needs I am facing now are:
When the motor is at rest, it is in a static state, but when I rotate it with my hand or load, it will generate resistance with a fixed torque. When my hand is released, it remains still.
How can I start? I noticed that in the lab5b project, I first turned off the forced angle and set the speed to 0. When I turned the motor by hand, the motor would slowly increase the torque along with the rotation of my hand, but after my hand was released, The motor seems to turn to the position where I started to rotate it. If I keep rotating it, it will shake or oscillate at a certain moment, but I think this project is close to my needs. How can I change this project to meet my needs? My product needs?
Thank you! Best wishes!