Hi Experts,
Customer is making the firmware which based on blinky_dc_cpu01 project under RAM_DEBUG build configuration. Recently, customer encountered Memory size issue. According to the following view, RAM0 and RAMLS0 was used, however RAMS1-RAMS4 are not used. I mean, they suppose they are able to use those RAM memories. Regarding "2837xD_RAM_lnk_cpu1.cmd" and "F2837xD_Headers_nonBIOS_cpu1.cmd" files, customer did not modify them. If customer should modify those cmd-files, could you elaborate how to fix them, please?
Also, I’m able to share this test-project offline, if you need it, please let me know.
And then, if you will share the helpful document which explains those memories, it would be appreciated.

Best regards,
Miyazaki