Other Parts Discussed in Thread: C2000WARE
Hello there,
I found TMS320F280049 group and even more powerful MSP430FR604x which seem as very good candidates for precise frequency measurement rather than regular MCUs which are slow (nanosecond resolution). I would like to hear your opinion to this measurement requirements.
I need to measure frequency ranging 1-2 MHz of a square signal with averaging over the period of 50 usec.
time measurement resolution: <1ns
period of one measurement: 50 usec
I need to measure frequency from number of edges of input square wave signal during this period (50 usec).
I would like to use HRCAP TMS320F280049 as described:
7.11.2 High-Resolution Capture Submodule (HRCAP6–HRCAP7)
The device contains up to two high-resolution capture (HRCAP) submodules. The HRCAP submodule measures the difference, in time, between pulses asynchronously to the system clock. This submodule is new to the eCAP Type 1 module, and features many enhancements over the Type 0 HRCAP module. Applications for the HRCAP include:
• High-resolution period and duty-cycle measurements of pulse train cycles
• Pulse-width capture in either non-high-resolution or high-resolution modes
or
I would use MSP430FR604x as described: High-precision time measurement resolution
Q1: Can TMS320F280049 / MSP430FR604x be used for such measurements?
Q2: Is there any working example for similar pulse signal measurements?
Q3: How does HRCAP for TMS320F2XXXXX measurement method works?
Q4: How does MSP430FR604x measurement method works?
Thank you for any help.
Best regards,
Michael