Hello. I'm currently using TMS320F28069 as the controller of my project and in the project, I need to use two interrupt for TIMER0 and TIMER1. When I read about the interrupt structure from the datasheet, I found that the interrupt signal of TIMER1 is directly sent into INT13 without entering PIE as shown below.
Presently, I have to modify the DefaultISR.c to set the interrupt function for Timer1 but I think it is not an elegant way. Other interrupts, who are controlled by the PIE block, can be set by changing the PIE configuration. So, I am wondering is there any way to assign the custom interrupt function for INT13 without changing DefaultISR.c.