Hi team,
Our customer developed current model with TMS320F28375D/SDRAM (IS42S16320F-7TLI :8M x 16 x 4 banks, 16bit Bus). For next system, customer plans to develop it with TMS320F28375D/ Two SDRAMs (IS42S16320F-7TLI :8M x 16 x 4 banks, 32bit Bus), like the attached file(Two_SDRAM_Implementation.zip). Therefore, customer is asking if it is possible to use a 32-bit bus EMIF with two SDRAMs. Can I have your expert's advice/comments on this, please?
If TI would Not be able to recommend this EMIF connection, can we have expert's advice how customer should implement two SDRAMs, please?
Best regards,
Miyazaki