CCS(Version: 10.0.0.00010)、デバッグ(虫マーク)でEEPROMにプログラム書き込みを実行すると下記エラーメッセージが出ます。本ターゲットボードは、電源電圧を定格を超える電圧まで上昇させてしまい、動作しなくなったが、破損したIC(2個)を交換した結果、動作するようにはなりましたが、プログラムの書き込み時下記のエラーが出てしまいます。CPUまで破損することは無いと思っていますが、どのような原因が考えられますか?
(ERROR MASSEGE)
Error connecting to the target:
(Error -180 @ 0x0)
The controller has detected a target power loss.
The user must turn-on or connect the power supply for the target.
(Emulation package 9.1.0.00001)