Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28377D: VDDA and VDD isolation

Part Number: TMS320F28377D

Hi,

I have a problem with my TMS. I want in a first part to supply the digital part then in a second part i want to use a GPIO to command the enable of the supply that will be use as VDDA. The problem is when i'm only suppling the digital part of my TMS320, i have 2.5V on the VDDA. So is that possible to supply the digital part in a first time then the analog part or do i need to suplly them simultaneously ?

best regards,

Greg