Part Number: TMS320F280049
Other Parts Discussed in Thread: REF3430
1. Do the ADC inputs have any type of clamping structure?
a. If so, to what voltage is it clamped to? (VDDA, VREFHI, other?)
b. F280049 datasheet Table 5-43, note 1 states that load current on VREFHI increases when ADC input is greater than VDDA. Could you explain or show an equivalent circuit for this?
2. Per datasheet, there is a warning to keep ADC inputs below Vdda +0.3 V. If the ADC inputs have a source impedance to limit the current into the clamp, is there an acceptable range of input current that will not upset the ADC, or associated ADC channels?
3. Why do they state that when using the ADC at a range of 0-3.3V the ADC will have reduced accuracy / precision?
4. When using the internal 3.3V ADC reference, what conversion results do you get when the ADC power rail is less than 3.3V but above the 3.3V reset (Micro continues to operate)? Will ADC results be adversely affected?
5. When using an external ADC reference:
a. Would I need to individually buffer each of the 3 VREFHI inputs (shown in ref manual below), or could all of these be tied together when using the REF3430?
b. How would this affect the use of the Device_cal{} function for ADC trim registers? Can they still be used?
c. How would using an external reference affect the post processing block for Offset Correction? Any issues?
d. If Device)cal() function is not used, is there intentional offset or deviation from ideal gain seen in the ADC channels?
e. When using Device_cal() or PPB offset correction, these only affect the raw ADC values, and cannot be used at the system scaling level, correct? (like module scaled voltage 0 to 48V, current 0 to 10A, etc).
f. If I want to achieve the largest ADC input range same as the F2837x, I would use an external reference of 3.0V, correct?
Thank you!