Hello,
My customer is trying to replace their STM32L010F4P6 (https://www.st.com/en/microcontrollers-microprocessors/stm32l010f4.html). I checked the cross-reference and couldn't find anything. I would like to pitch an MCU that has >= pins, max frequency, etc. Also, it must have built in bootloader so it can be programmed over UART. The main essentials are that it is able to accurately measure frequencies up to ~200kHz, and then generate a PWM output for firing our IR markers at ~50khz. We use 2 analog inputs, and a few more simple GPIOs.
Any recommendations?
Best,
Alex