Hi!
I've some problems flashing a TMS570LS3135 device with nowFlash v3.41. I use a Spectrum Digital XDS510USB debugger and get the following error message:
A quick check of the nowFlash.cfg file shows, that the device ID 0x802AAD05 identifies the configuration sections for a TMS570LS3137, a TMS570LS2125 and a RM48L950. I am not sure which of these sections is applied but no configuration sets the right cpu frequency for this device which I've overwritten from the nowFlash GUI to be 160MHz:
I'he also checked that "Scan Chain 0" is disabled and Big Endian is enforced in the configuration of the XDS510USB. I also tried to use the -w option with values from 1 to 10 with no success.
Could someone give me a hint, whats going wrong here?
Thanks in advance,
Christoph