Part Number: HERCULES_SAFETY_MCU_DEMOS
Hello!
I installed Hercules Safety MCU Demos to study the Safety features of the RM57Lx LaunchPad.
Firstly im not 100% sure which exe is needed to run in order to run the demo on the RM57Lx LaunchPad.
Am I right that the selected one from the installation folder is the one for me to run?
After I run it the application don't start but it misses a DLL file. You can see it on the next picture.
I tried downloading the missing DLL but that didn't work. If i clicked to ignore it the app started but it didn't work.
Can you suggest me any solution for this problem problem, or help me anyhow to study the safety features of this chip.
Regards,
Aron