Part Number: HERCULES_SAFETY_MCU_DEMOS
Tool/software: TI C/C++ Compiler
Hi,
I'm configured SPI1, SPI2, SPI3 and SPI4 use Halcogen. SPI1, SPI3 and SPI4 work very good, but i have some problems with SPI2.
When i use spiTransmitAndReceiveData(spiBASE_t *spi, spiDAT1_t *dataconfig_t, uint32 blocksize, uint16 * srcbuff, uint16 * destbuff), the transmission fail at first byte:
Spi->IntFlg = 0x01000210 = BITERRFLG is 1. I try one SPI for time, i try to send same message.
Can you help me please?
p.s: I use SPI2 without any slave in this moment, i view signals with oscilloscope.