Part Number: HERCULES_SAFETY_MCU_DEMOS
Hello, I am a beginner trying to get I2C to work on the TMS570LC43x Microcontroller and I am using the code provided in the "example_i2cMaster_TX_RX.c" file. I use the functions generated by HalCoGen and configure it as instructed in the example. I am getting stuck in an infinite loop (pictured below). I am not sure how to fix it.
/* Include Files */ #include "HL_sys_common.h" /* USER CODE BEGIN (1) */ #include "HL_i2c.h" /* USER CODE END */ /** @fn void main(void) * @brief Application main function * @note This function is empty by default. * * This function is called after startup. * The user can use this function to implement the application. */ /* USER CODE BEGIN (2) */ #define DATA_COUNT 10 #define Master_Address 0x26 #define Slave_Address 0x40 uint8_t TX_Data_Master[10] = { 0x10,0x11,0x12,0x13,0x14,0x15,0x16,0x17,0x18,0x19}; uint8_t RX_Data_Master[10] = { 0 }; uint8_t TX_Data_Slave[10] = { 0x20,0x21,0x22,0x23,0x24,0x25,0x26,0x27,0x28,0x29}; uint8_t RX_Data_Slave[10] = { 0 }; /* USER CODE END */ int main(void) { /* USER CODE BEGIN (3) */ int repeat = 0; int delay =0; /////////////////////////////////////////////////////////////// // Master Transfer Functionality // /////////////////////////////////////////////////////////////// /* I2C Init as per GUI * Mode = Master - Transmitter * baud rate = 100KHz * Count = 10 * Bit Count = 8bit */ i2cInit(); /* Configure address of Slave to talk to */ i2cSetSlaveAdd(i2cREG1, Slave_Address); /* Set direction to Transmitter */ /* Note: Optional - It is done in Init */ i2cSetDirection(i2cREG1, I2C_TRANSMITTER); for(repeat = 0; repeat < 2; repeat++) { /* Configure Data count */ /* Note: Optional - It is done in Init, unless user want to change */ i2cSetCount(i2cREG1, DATA_COUNT); /* Set mode as Master */ i2cSetMode(i2cREG1, I2C_MASTER); /* Set Stop after programmed Count */ i2cSetStop(i2cREG1); /* Transmit Start Condition */ i2cSetStart(i2cREG1); /* Tranmit DATA_COUNT number of data in Polling mode */ i2cSend(i2cREG1, DATA_COUNT, TX_Data_Master); /* Wait until Bus Busy is cleared */ while(i2cIsBusBusy(i2cREG1) == true); /* Wait until Stop is detected */ while(i2cIsStopDetected(i2cREG1) == 0); /* Clear the Stop condition */ i2cClearSCD(i2cREG1); /* Simple Dealya before starting Next Block */ /* Depends on how quick the Slave gets ready */ for(delay=0;delay<1000000;delay++); } while(1); /* USER CODE BEGIN (4) */ /* USER CODE END */ return 0; }
The loop which I get stuck in is in the i2cSend() function.
void i2cSend(i2cBASE_t *i2c, uint32 length, uint8 * data) { uint32 index = i2c == i2cREG1 ? 0U : 1U; /* USER CODE BEGIN (17) */ /* USER CODE END */ if ((g_i2cTransfer_t[index].mode & (uint32)I2C_TX_INT) != 0U) { /* we are in interrupt mode */ /*SAFETYMCUSW 45 D MR:21.1 <APPROVED> "Valid non NULL input parameters are only allowed in this driver" */ g_i2cTransfer_t[index].data = data; /* start transmit by sending first byte */ /*SAFETYMCUSW 45 D MR:21.1 <APPROVED> "Valid non NULL input parameters are only allowed in this driver" */ i2c->DXR = (uint32)*g_i2cTransfer_t[index].data; /*SAFETYMCUSW 45 D MR:21.1 <APPROVED> "Valid non NULL input parameters are only allowed in this driver" */ g_i2cTransfer_t[index].data++; /* Length -1 since one data is written already */ g_i2cTransfer_t[index].length = (length - 1U); /* Enable Transmit Interrupt */ i2c->IMR |= (uint32)I2C_TX_INT; } else { /* send the data */ /*SAFETYMCUSW 30 S MR:12.2,12.3 <APPROVED> "Used for data count in Transmit/Receive polling and Interrupt mode" */ while (length > 0U) { /*SAFETYMCUSW 28 D MR:NA <APPROVED> "Potentially infinite loop found - Hardware Status check for execution sequence" */ while ((i2c->STR & (uint32)I2C_TX_INT) == 0U) /* GETTING STUCK HERE */ { } /* Wait */ /*SAFETYMCUSW 45 D MR:21.1 <APPROVED> "Valid non NULL input parameters are only allowed in this driver" */ i2c->DXR = (uint32)*data; /*SAFETYMCUSW 45 D MR:21.1 <APPROVED> "Valid non NULL input parameters are only allowed in this driver" */ data++; length--; } } /* USER CODE BEGIN (18) */ /* USER CODE END */ }
What can I do to fix this?