Hi experts,
The Safegy Manual mentions the Diagnostics P1T5A, P1T5B, P2T5A, P2T5B, P3T5A, P3T5B which are called "Boot Time Software Test of Basic Functionality Including Error Tests" or "Periodic Software Test of Basic Functionality Including Error Tests". I am not sure what exactly should be tested by this diagnostic. I had a look at the SafeTI Library which has no direct emntion of this diagnostic. Assuming it is thesame Diagnostic, I had a look at the implementation "SL_SelfTest_PeripheralSegmentInterconnect" function which tests the correct function of reserved mode and protected mode.
(Q1) Does the P1T5A refer to testing if it is possible to access a reserved location and possible to write to a protected location?
Thank you and best regards,
Max