Hi,
I am starting on a Hercules project. I downloaded your example spna183.zip and flash_defines.h is missing. Where would I find it for the RM46L830 processor?
Thanks, Steve
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I am starting on a Hercules project. I downloaded your example spna183.zip and flash_defines.h is missing. Where would I find it for the RM46L830 processor?
Thanks, Steve
Sorry, that project was built with an older version of the F021 API library and it used absolute path information. Here is what I did to get it to compile and link. The include paths I used are based on where I unzipped the source files. In my case I unzipped to "c:\ti\Hercules". I changed the build settings for the include files from:
to:
I changed the linker "File Search Path" from:
to:
I then deleted the "bl_link.cmd" file that was in the project and added to the project this modified version of bl_link.cmd. The corrections I made were to remove the "..\release\" in front of the two specified object files and to correct the flash size for the RM46 device.
/cfs-file/__key/communityserver-discussions-components-files/312/6406.bl_5F00_link.cmd