This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

TMS570LS0232: TMS570LS0232

Prodigy 220 points

Replies: 2

Views: 210

Part Number: TMS570LS0232

Hello Sir,

I have recently downloaded the Cortex R4 processors hardware toolbox setup and have downloaded all the software required. But I'm not able to "Update Firmware" during Support package installer, where I get the error :

The value is '-260' (0xfffffefc).
The title is 'SC_ERR_XDS110_OPEN'.

The board and the USB connection is fine, as the code was dumped on it to check the launchpad. Do explain what the error means and how to sort it.

Thank you,
Sushma Mantagani

  • Is this error from TI or MathWorks software?  If it's for TI software, this is the right place to ask.  

    If its for MathWorks software, go to MathWorks Technical Support.

    -Brian

    Brian McKay  |  Technical Marketing  |  www.mathworks.com

  • Hello Sushma,

    As Brian has mentioned, please post the question in thier online support if this is an error received from that toolset. Most of what you have stated is unrecognizable to me so I am assuming it is the Mathworx tools. Also, please clarify which Hercules device you are using. We do not have a Launchpad with the TMS570LS0232 device on it; however, we do have one with the TMS570LS0432. The two are 100% compatible except the LS0232 has less flash memory.

    Brian,
    Thanks for jumping and helping to redirect for the better support.

    Thanks and Regards,

    Chuck Davenport

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.