This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Replies: 7
Views: 710
Part Number: TMS570LS0232
Hello Team,
I have a customer who wants to start a new design with Hercules family.Thier application needs are very simple but the requirement of working temperature range must be -40 up to + 125 degrees.I found that this family supports desired temperatures and automotive interfaces like CAN and LIN as well.In addition, there is a requirement of using SD Card when SPI MODE should be more than enough (so far so good).
My questions are:
whether this family is recommending for a new design? I found out this family support was drop out from CSS 7 and examples are limited?
This cause to the customer for a bit concern for lack of examples and support.
additionally, there is a need to add a small LCD display if the device support that?
Can you please advise for the above, Thanks
Best regards,
Shai
In reply to Sunil Oak:
In reply to Shai Berman: