This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Replies: 6
Views: 719
Part Number: TIDM-TMS570BMS
Hi I was looking at www.ti.com/.../TIDM-TMS570BMS design and was wondering if anyone could help me identify the board that the batteries are all connected to or maybe a family of similar boards. Thank you in advance.
Best regards,Tom
If I had answered to your question, please mark this post as Resolved.
In reply to Tomasz Kocon:
Yes the batteries are 18650 Lithium Ions but what I want to know is the board theyre connected on, the battery board with 3x16 battery slots in this picture:
In reply to Reynier Serpa:
Thanks and Regards,QJ Wang
For more information: Hercules FAQ
In reply to QJ Wang:
Those are the components that I was already familiar with, however my question is mostly on what looks like a yellow board on the TMS570LS0432. If anyone could identify what that is then that would be much appreciated. There also seems to be two cables coming from the yellow part into the EM 1402 EVM. If anyone could identify those aswell that would be great. I believe that one of them is some sort of UART connector.