Hi Team,
We are using Hercules TMS570LS3137 controller with CCS8.0. We are using the HET module for below functionality.
Configure PCNT instruction for reading the pulse counts and read the pulse count values for certain number of events.
Now, if we implement the above functionality for multiple HET pins, we are seeing abnormal behavior when following conditions happen:
1. Our primary requirement is that when no input signal is given to HET pins, the pulse count values should be read as 0. So, for this, we enabled control feature.
2. When we remove input on one of the HET pin (say 0) and given valid input for other HET pin (say 1), and wait until control field value for PCNT instruction on pin 0 reaches to all 1's.
3. Now, reading pulse count value from pin 1 is not a valid one.
Can you please let me know the reason for this behavior and is there any errata and work around for this issue?
Regards,
M.Sreenivasan.