Hello,
I downloaded the package SAFETI-HERCULES-DIAG-LIB-CSP-DEMO to understand what this toolkit provides and what we might need to add to the test suite.
I have followed the instructions for the installation of the package. I already had the compiler CCS V8.0 installed.
I tried to run the script "ldra_execute.bat" and ended up with this error message:
C:\Program Files (x86)\LDRA\LDRAunit-TI-Qual_C_CPP_9.4.3\Compiler_spec\Ticcs50\Rm48l950_hercules_serial>ldra_execute.bat
Usage: loadti [OPTION]... [OUT_FILE1[+OUT_FILE2]...] [ARGUMENT]...
Load OUT_FILE executable(s) to TI target and run, passing ARGUMENT(s) to main.
Mandatory arguments to long options are mandatory for short options too.
Options:
-a, --async-run
-b, --init-bss-section[=VALUE]
-c, --cfg-file=CONFIG_FILE
-h, --help
-l, --load
-mlr, --mem-load-raw="PAGE,ADDR,FILE,TYPE_SIZE,BYTE_SWAP"
-mld, --mem-load-dat="PAGE,ADDR,FILE,LEN"
-msr, --mem-save-raw="PAGE,ADDR,FILE,LEN,TYPE_SIZE,BYTE_SWAP"
-msd, --mem-save-dat="PAGE,ADDR,FILE,LEN,IO_FORMAT,APPEND"
-n, --no-profile
-q, --quiet
-r, --reset
-s, --stdout-file=FILE
-t, --timeout=VALUE
-v, --verbose
-x, --xml-log=FILE
-@, --options-file=FILE
One point to precise: I don't have a dev kit connected to my PC.
Question #1: Why do I get this error message? Is it because it doesn't find a dev kit or because of something else? It is not clear what is the problem.
I then tried to select the tests to run directly from LDRA, as per the user manual SafeTIHerculesDiagnosticLibraryTAU_User_guide.pdf, figure 6, 7, and 8 (page 10-11). The dialog box shown at Figure 8 doesn't present any sets to select - it is completly empty.
Question #2: Is it possible that there is an issue with my installation?
I then wanted to open the TCF files of the CSP directly in LDRA, to be able to visualise the tests being performed, but couldn't find them on my PC.
Question #3: Where are the TCF files installed?
Thank you in advance for your assistance with those issues.
Kind regards,
Frederic.