Other Parts Discussed in Thread: TMS5701224, TMS570LS1224
We use pin25 for a clock output and pin30 for a signal output. These two single are for Flash and FRAM. We find these signal can work normal in 25deg.C ~ -30deg.C, but it will fail in -40deg.C. We check the waveform that have big noise spike during pulse on/off. In the meantime, the high level voltage will drop from 3.3V to 3V. (We have check the VCC of pull high voltage is 3.3V.)
(1)at 25 degree C
(2)at -40 degree C
TMS5701224 side:
Flash、FRAM side:
BR,
Gary