Tool/software: Code Composer Studio
I want to use Hercules SafeTI Diagnostic Library.
I use TMS570Lc4357 board - development kit.
Hercules SafeTI Diagnostic Library version is "2.4.0". So i build the TMS570LC4357_NoOS.
I use the Debug as "Texas Instruments XDS100v2 USB Debug Probe". Then I result is stop in this function(the green color line).
------
boolean SL_ESM_nERROR_Active(void)
{
boolean retval = FALSE;
/*SAFETYMCUSW 134 S MR: 12.2 <APPROVED> Comment_4*/
if(ESM_ERROR_PIN_OFF == BF_GET(sl_esmREG->EPSR, BF_EPSF_START, BF_EPSF_LENGTH)) {
retval = FALSE;
}
else {
retval = TRUE;
}
return(retval);
}
-----
What is the problem the code is stop in this line?