Hi,
I am working on the Hercules TMS570LC4357 Development Kit.
But after loading some program i have observed that the controller is heating so much like burning the finger(but able to load the image).
I have checked but there is not shorting of the board. 4 blue led's beside the power button are glowing along with the usb light. but also one red error light is glowing.
It is not just while loading, but if just connect the power supply it is heating too much.
I have applied isopropyl alcohol solution to it but of no use.
It seems that the controller is going into reset continuously after loading.
Can anyone please help me in this?
Regards,
Shivam Kakad