This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

TMS570LS1227: What is the difference between soft restart and power on restart after power down

Expert 5605 points

Replies: 2

Views: 105

Part Number: TMS570LS1227

Dear team,

Could you please tell me what is the  difference between soft restart and power on restart after power down?

Recently my customer encountered a problem as below,

Our device's I2C connect an E2PROM , our device and the E2PROM shares one power supply 3.3V. When the first power-on 570‘s boot fails to read the eeprom, and read three times, all failed to read. And then 570 did a soft restart, then continue to read, but still failed. When the fault happens, the SCL and SDA's waveforms are abnormal(is always high). Only when the power is turned off and then powered on can read successfully.

So I want to know what is the difference between soft restart and power on restart after power down.

Thanks & Best Regards,

Sherry

  • Hi Liang:

    You can check the TMR of the TMS570, Section 12.2.1 "Reset Behavior", which is a description of the difference between soft reset and power-down reset. But I don't think this has anything to do with the processor. I have encountered similar problems before, which is caused by the unreasonable peripheral circuit design of the device. Some of the Electric is not be released quickly.

  • In reply to MichaelLee:

    Hi,

    Ok, got it! Thank you!

    Thanks & Best Regards,

    Sherry

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.