Tool/software: TI C/C++ Compiler
Hi all,
in our project from the beginning we have been using the following aliases for data types:
typedef signed int sint32_t; /* Signed 32-bits integer (signed int/) */
typedef unsigned int uint32_t; /* Unsigned 32-bits integer (unsigned int) */
Now we faced with a necessity to change it to the following:
typedef signed long sint32_t; /* Signed 32-bits integer (signed long) */
typedef unsigned long uint32_t; /* Unsigned 32-bits integer (unsigned long) */
I would like to ask, can we expect some side effect in case of such a change or int/long type are absolutely equal to each other?
Compiler version is TI ARM 18.12.0.
Thanks in advance!