Other Parts Discussed in Thread: HALCOGEN
We're updating a product that was released with code generated from HALCoGen v4.07.00 to use code generated from HALCoGen v4.07.01.
Our release process includes review and analysis of all known issues with third-party tools and code used to generate our firmware.
v4.07.00 used a format such as "SDOCM00084753" for its errata references, while v4.07.01 uses a format such as "HERCULES_SW-5082". It is not clear to us in all cases how to map between these references.
Can you please help us align these references properly so that our errata tracking / analysis is correct?
Here is where we are currently at:
v4.07.00 References | New-format References | Status in v4.07.01 | Description |
SDOCM00084753 | SYS: Since the PLL tab does not spit out warnings if any final or intermediate frequencies generated are out of spec. | ||
SDOCM00086009 | Tool: No KEIL tool support for TMS470M devices | ||
SDOCM00087899 | FEE: The FEE driver GUI in TMS470Mx family only supports 10 blocks. | ||
SDOCM00095488 | CAN: Support for Mixed mode in can driver is necessary. | ||
SDOCM00088096 | ADC: interrupt Enable check box for Event, Group1 and Group2 groups for ADC1, ADC2 in HCG. | ||
SDOCM00122504 | FEE: HALCoGen FEE Driver Does Not Set Bank Before Writing To Flash. | ||
SDOCM00122496 | FEE: HALCoGen FEE Corruption - Block Header Not Written Properly. | ||
SDOCM00122164 | SYS: HALCoGen RAM and Stack Locations are Hard-coded. | ||
SDOCM00121738 | FEE: FEE Driver Does not Check CRC when reading and crc option is enabled. | ||
SDOCM00122382 | SYS: Clock Tree tab to RM57 and TMS570LC43 are not available. |
--thx