Dear team of the Hercules Support,
Would you please explain how are the uncorrectable ESM Errors 2.3, 2.19 and 2.21 related to each other?
And the correctable errors 1.4 and 1.6 respectively?
It still isn't plain to me who is issueing each of these errors and in which cases one of these errors is issued.
(Q1) For example, is the 2.19 issued only on implicit OTP reads and not on CPU reads/instructon fetches on the flash?
(Q2) What's the difference between the errors 2.3 and 2.21 in terms of issuer and conditions?
(Q3) Are both errors 2.3 and 2.21 results of a bus event 0x71 with EVNTBUSm bit 48 set?
(Q4) Which of these errors will occur during the test FLA11 using DIAGMODE 7?
Thank you in advance for your support - enjoy the weekend!
Stephan