This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61030: Did I make a design issue with my BQ24075+TPS61030 based power supply

Part Number: TPS61030
Other Parts Discussed in Thread: BQ24075, TPS61031, TPS61032

I made a power supply (not my expertise) based around the TPS61030 boost converter and BQ24075 battery charger. The power supply should normally be coming from a regulated 5V USB charger (USB-C), but also contain a single li-ion battery for backup power. On the output side it should be able to provide 2A at 5V. The power supply is part of a larger PCB that includes a lot more components. The first prototype of this PCB came in and after powering up fine initially, after a minute or so it shuts off and won't power on anymore. At that point, if I connect a 5V bench power supply to it, there is a 2V voltage drop straight away, which I think indicates a short/fried component somewhere. But on the power supply side (or anywhere else for that matter) I see no swollen capacitors, magic smoke or any other visual or olfactory signs of components failing. So the issue could be in a few places, but for now I would like to ask if I made any clear mistakes in the power supply design. During the test, only the 5V USB power supply was connected, and no battery. The second time I tested it (with a fresh board and same results) the 5V USB power supply came from a bench power supply and it never seemed to draw any excessive current. It stayed well below 1A as far as I saw (I didn't see it above 500mA even).

This is the power supply part of my schematic:

and these are the board layouts (2 layer board only), top (the U1 marking disappeared, but it is the only other IC on there, and L1 is the big component under C16 and U4, which is a Bourns 6.8uH inductor SRN8040TA-6R8M):

and bottom: