I need to qualificate test about SafeTi Diagnostic Lirary using by TMS570LC4357.
So, I request SafeTi Diagnostic Lirary using by TMS570LC4357 in "Ti home page". I received "SafeTI Diagnostic Library-tau-TMS570LC43x-2.4.0_LDRA_Less-installer.exe"
Install this package, I can show the report of SafeTi Diagnostic Lirary using by TMS570LC4357 tested by Ti. But I need to test by myself.
when I try to test by myself, there are some problems,
First, my test environment.
1. Hardware : Our configured board (The board is made as ti guide. We already use the SafeTi Diagnosis Library well)
2. Software
1) Use the project in "SafeTI Diagnostic Library-tau-TMS570LC43x-2.4.0_LDRA_Less-installer.exe"
2) LDRAUnit set as the user guide.
3) Complier use "ccs8" -> so, the complier use "ti-cgt-arm_18.1.4.LTS"
The changed Test environment
1. Sci port : We use Sci port 4 in TMS570LC4357
1) I set bit 17 of sciREG4->GCR1 by following the guide ("HL_sci.c" in the root "C:\ti\Hercules\SafeTI Diagnostic Library\2.4.0_LDRA_Less\demo_app\HALCoGen\TMS570LC4357_NoOS\source")
2) sciREG1 -> sciREG4 in "ldra_port.c" in the root "C:\ti\Hercules\SafeTI Diagnostic Library\2.4.0_LDRA_Less\Test\TMS570LC43x\SafetyLibrary\Tests\source"
2. Change the Cmd file
-> Build is failed, when I use "SL_TMS570LC4357_NoOS_sys_link.cmd" in "C:\ti\Hercules\SafeTI Diagnostic Library\2.4.0_LDRA_Less\Test\TMS570LC43x\SafetyLibrary\Tests\source"
So, I use "SL_TMS570LC4357_NoOS_sys_link.cmd" in "C:\ti\Hercules\SafeTI Diagnostic Library\2.4.0_LDRA_Less\build\TMS570LC4357_NoOS"
Then, the test is stopped following state,
The Debugger is stopped when system reset state.
Please let me know, why the system is stopped in this state.
Regards,
Minwoo