Please can someone point me to documentation defining the minimal interface requirements for initial software programming of a TMS570LS0232. Also, what are the minimal JTAG requirements for emulation? Is it possible to get the pin count down to a 10 pin Tag-connect header? (e.g. single 3.3V, single 0V reference, EMU0 and EMU1 combined as one pin)
My understanding is that a 14 pin connector is required to interface with a JTAG / programming tool to allow initial flash programming on a PCB. Are all 14 pins required, and what are the pull-up / pull-down requirements. If I'm programming only, do I need anything more than the 7 JTAG connections (Test, TMS, TDI, TDO, TCK, RTCK and nTRST) plus 0V reference?