I need the certification of SafeTI Diagnostic Library. So, I requested Ti and received "SafeTI Diagnostic Library 2.4.0_LDRA_Less".
I buy the LDRA Unit and run the project in "SafeTI Diagnostic Library 2.4.0_LDRA_Less". But it was build fail.
I wonder what's problem of act this project.
- I test method and result as followes,
1. I just change the complier as "ti-cgt-arm_18.1.4.LTS"
2. Here is the Log the build fail of ADC test (
- The other test is same
Regards,
Minwoo