I have an XDS200 which I use together with IAR EWARM connected to my TMS570LC4357 board.
If I move the XDS200 to my Linux system running Ubuntu-18.04
It has a CCS 10.2 installation where I installed all three choices for probes.
Have run ccs1020/ccs/install_scripts/installdrivers.sh
=====
When I insert the XDS200 in the Linux PC in a USB slot in the backpanel,
I can see that the driver seems to load OK.
$ dmesg:
[235647.855823] usb 2-1.2: new high-speed USB device number 19 using ehci-pci
[235647.964686] usb 2-1.2: New USB device found, idVendor=0451, idProduct=bef0, bcdDevice= 1.00
[235647.964688] usb 2-1.2: New USB device strings: Mfr=1, Product=2, SerialNumber=3
[235647.964690] usb 2-1.2: Product: XDS2xx USB Emulator - Composit
[235647.964691] usb 2-1.2: Manufacturer: Spectrum Digital
[235647.964692] usb 2-1.2: SerialNumber: S200-000E99039000
[235647.986423] cdc_acm 2-1.2:1.0: ttyACM0: USB ACM device
[235647.986841] cdc_acm 2-1.2:1.2: ttyACM1: USB ACM device
[235647.987078] usbcore: registered new interface driver cdc_acm
[235647.987079] cdc_acm: USB Abstract Control Model driver for USB modems and ISDN adapters
=====
I then define a target with a TMS570LC43xx and the USB XDS2xx probe
When I test the connection I get the following:
==================================================================
[Start: Texas Instruments XDS2xx USB Debug Probe]
Execute the command:
%ccs_base%/common/uscif/dbgjtag -f %boarddatafile% -rv -o -S integrity
[Result]
-----[Print the board config pathname(s)]------------------------------------
/home/ulf/.ti/ccs1020/0/0/BrdDat/testBoard.dat
-----[Print the reset-command software log-file]-----------------------------
This utility has selected a 560/2xx-class product.
This utility will load the program 'xds2xxu.out'.
<Long pause>
E_RPCENV_IO_ERROR(-6) No connection: DTC_IO_Open::dtc_io
Failed to open i/o connection (xds2xxu:0)
An error occurred while soft opening the controller.
-----[An error has occurred and this utility has aborted]--------------------
This error is generated by TI's USCIF driver or utilities.
The value is '-250' (0xffffff06).
The title is 'SC_ERR_ECOM_EMUNAME'.
The explanation is:
An attempt to access the debug probe via USCIF ECOM has failed.
[End: Texas Instruments XDS2xx USB Debug Probe]
==================================================================
There is no "xds2xxu.out" in the installation. There is an xds2xxu_io.so
Have tried to run dbgjtag manually with no better result.
What to do?