This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430F2619S-HT: Operating the device at 3.8V

Part Number: MSP430F2619S-HT

Hi Team,

The absolute maximum operating voltage of MSP430F2619SPM is 4.1V as stated in the datasheet and the recommended operating condition is 3.6V (max). Our customer would like to know if there are any concerns or significant degradation to MTBF of this device if it is operated continuously with 3.8V applied to VCC. If they operate the device in this condition continuously, should they be concerned about degraded reliability or will this part continue to operate as expected?

Regards,

Danilo

**Attention** This is a public forum