Other Parts Discussed in Thread: LP3982, TIDA-01172
I am running an msp430fr5969 at 1.8v (I have the LP3982 circuit configured for start-up conditions - similar to TIDA-01172).
In order to program this chip, I can not use the debugger or usb since those are at 3.3V.
I am looking at using UART (MSP430FRBoot) however the MSP430FRBoot – Main Memory Bootloader and Over-the-Air Updates for MSP430 FRAM (Rev. E) -section 5.3 mentions that a 3.3v voltage source must be used. If this is true, how can I program the MSP430fr5969 chip at 2V?
Can I use a logic level shifter?