Hi,
A crystal with a load capacitance (Cload) of 7pF is connected, the internal Cl, eff = 5.5pF is set, and a 4pF capacitor is added to the Xin and Xout terminals (Cl1, Cl2).
Currently, we are considering changing to another manufacturer's product.
I'm thinking of a load capacitance of 12.5pF, but if I leave Cl, eff = 5.5pF above, is it okay if the external capacitor capacitance is 15pF?
(Ultimately, the manufacturer will check the matching, but I want to know the default setting before that)
Thanks,
Koki