I am trying to flash the transform_ex1_fft_fixed_q15 example from the DSP Library for MSP430 (Library). When I try to flash it, I get the error mentioned in the title. Looking at other threads (Related question), I tried to change both my stack and heap sizes so that the main file would build and I could look at the map file. However, trying stack and heap sizes anywhere from 5 to 1000 (originally 160), did not work. I've tried looking at the memory allocation tab. Failed allocation states "160 out of -1 bytes used (-16000%)", RAM states "2,408 out of 2,408 bytes used (100%)", FRAM states "110 out of 48,000 bytes used (0%)", and FRAM2 states "4,338 out of 81,912 bytes used (5%)". Available memory ranges are:
RAM size: 0x800 unused: 0x0 max hole: 0x0
I have also tried using a second MSP430FR6989, but I get the same error. Does anyone know how else I can see what is causing this error, or if my MCU simply doesn't have enough FRAM (128kB)?