Is it possible to increase the signal sampling frequency in the USS GUI above 8MHz? I am using 2.2MHz transducers and getting inaccurate results because of the too slow sampling rate. My ADC capture has a large DC offset and my absolute TOF readings appear to be quantizing around 125ns which is the 8MHz sampling rate. Is there any way to increase this?
Thank you!