Other Parts Discussed in Thread: MSP-FET
Using CCS v10 and an MSP430F5638 running on a custom SBC driving an LCD. Code, board, and LCD were running fine. Using MSP-FET to program the MCU.
Normal use:
Build code ok, Run Debug and the program used to run fully from the Step Return Arrow, then pick the Terminate button to exit the debugger and return to the IDE.
Current use:
Press Step Return Arrow and LCD shows junk, and program stalls, then pick Terminate and the program runs completely and correctly, showing correct data on the LCD.
Why is the behavior different?
Also I can't single step into the program, getting the following error message:
MSP430: Can't Single Step Target Program: Could not single step device