Using the built-in AD24 bit sampling, the direct voltage acquisition zero drift is about 5,6 mV. The environment is not disturbed, just the bare board test, both of them. Why?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Using the built-in AD24 bit sampling, the direct voltage acquisition zero drift is about 5,6 mV. The environment is not disturbed, just the bare board test, both of them. Why?
Hi 人在江湖
Please check Eos parameter on DS
May I know which GAIN setting you are using
and please check the test method on notes (4) after the Table 5-42, Please help to follow this measurement method and check if the Eos is the same with DS parameter
Thanks!
**Attention** This is a public forum