Other Parts Discussed in Thread: ENERGIA,
I found this problem happened for a long time before but seems not being solved at all.
I just download Energia 1.8.11E23 version and also install ti_msp430driver_setup_1.0.1.2.exe on windows 10.
When I start Energia IDE and start to do sample code with couple lines, but don't work with Serial.print(). This bug seems being introduced for a long time before.
I check following thread with no solution and was closed. Very strange !
>>> MSP-EXP430G2ET: Serial.print() not working. Nothing is being printed on Serial Monitor <<<
https://e2e.ti.com/support/microcontrollers/msp-low-power-microcontrollers-group/msp430/f/msp-low-power-microcontroller-forum/757445/msp-exp430g2et-serial-print-not-working-nothing-is-being-printed-on-serial-monitor
My setting as follow:
OS: Windows 10 Pro
IDE: Energia 1.8.11E23
USB driver: msp430 1.0.1.2
Board: MSP430G2ET launchpad
There will be two serial com port found on system after installed into PC.
1. MSP Application UART1 (COM15)
2. MSP Debug interface (COM14)
I also follow instruction from the post to switch pin TXD, RXD from vertical to horezontal, nothing working so far. Is that a bug that was not taken care for 3 years ??
this post seems to be asked on 2018 ....
That's ridiculous for such a BIG COMPANY line TI ?? Or you just simply don't care ?
-tommy