Good Morning,
It seems that there are a whole lot of information available on BSL usage and it is a bit difficult to sift through the available info.
What I am looking for is to exercise the BSL from a command line via UART interface. I am not sure if I can be using the BSL scripting.
Currently, the system that I am using is UART0 (eUSCI_A) for the serial comms @ 115K bit rate.
It is capable of performing full duplex transactions. Based on some of the info I read, I can invoke the BSL via an application command.
That said, would you please help in directing me with:
* A sample program that exercise BSL via command line, NOT bsl script. I'm using the UART Rx/Tx/GND lines only and most likely due to this BSL scripting would not work. If it does, please include that option too.
* A guide or appnotes ...
Thank you in advance for your help and support.
Best regards,
Ziggy