The TI E2E™ design support forums will undergo maintenance from July 11 to July 13. If you need design support during this time, open a new support request with our customer support center.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Use MSP430 + Accelerometer + Rechargeable Battery in a Wristband? Need help ensuring components.

Other Parts Discussed in Thread: CC430F6125, MSP430BT5190

Hi there.

I am attempting to figure out the costs of producing a wristband with the MSP430 (CC430F6125) and some additional components so that it would be able to do:

  • 3 axis (possibly 6 axis) accelerometer sensing
  • bluetooth
  • some flash memory
  • rechargeable battery

From what I understand, the MSP430 package already contains the bluetooth and flash memory, so is it correct that I only need to (essentially) plug in an accelerometer chip and some sort of rechargeable power supply? Would I need to purchase any other components? I am looking at the moment at a ADXL346 accelerometer.

Thanks,

Will

  • William,

    TI's bluetooth solution is not provided with the CC430F6125. It is only possible to use the MSP430BT5190. The CC430 already contains a sub 1GHz transceiver. You can find more information here:

    http://processors.wiki.ti.com/index.php/MSP430_Bluetooth_Platform

     

    Gustavo

     

     

  • Thanks for the information. So with the MSP430BT5190, all I need to do is fit a rechargeable battery and accelerometer? I don't know much about fitting components into a system, but I presume the bulk of the cost of producing such a system, in terms of the components, would be with the battery, accelerometer, and the MSP430? Is there anything else required for making a device that could store accelerometer data, transmit the data via bluetooth, and be recharged?

  • William,

     

    It really depends on a lot of things. For example, there is a cost of PCB and also assembly, unless you use what is given and don't customize it. The EZ430-RF2560 already does most of what you want. It has an accelerometer that it uses to transmit data via bluetooth. This is used in our Tux Racer demo. In that case, you would just need to add a rechargeable battery.

     

    Gustavo

  • Sounds good. Thank you very much.

**Attention** This is a public forum