Hi,
According to this memory map for ultrasonic sensing, can I be able to implement MSP430FRBoot to add the OAD feature?
Thank you
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
According to this memory map for ultrasonic sensing, can I be able to implement MSP430FRBoot to add the OAD feature?
Thank you
Hi Dushan
Could you give more details about OAD feature? If you want to realize the bootloader function we do have BSL to do this.
Hi,
Thank you for the reply.
I want to add the Over the Air firmware update feature to the ultrasonic flow rate project. I found that we can perform OAD with MSP430FRBoot. But my problem is, will I be able to implement MSP430FRBoot with this ultrasonic project, because of the lack of memory space in FRAM
Yes that is fine, I saw there are 1.4k RAM left can be used for OAD. That is enough to cash one more packages send by host.
Thank you for the reply,
But I saw OAD implementations using FLASH only. Can you send some documents regarding implant OAD with RAM
But my problem is, will I be able to implement MSP430FRBoot with this ultrasonic project, because of the lack of memory space in FRAM
As I mentioned that we have BSL to this, the BSL is a internal bootloader in ROM memory. More information you can refer to this user's guide
If you don't want to use hardware invoke and to use software invoke you can also refer this
**Attention** This is a public forum