Part Number: MSP-EXP430G2
HI folks,
I found old launchpad MSP-EXP430G2 and tried to use it in a some project. I've tried to connect it to CCS 10 (latest) on Ubuntu 20.04, but it can't be detected. The same board works on the same PC if I use CCS 10 in Windows 10 (can flash and debug).
I checked output of lsusb in Ubuntu, which indicates that USB drivers are in place. Does anyone have a hint why I can't load binary and run debugger in Ubuntu?
Regards