This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430FR4133: Coding the pins for the LCD screen with HDC2010EVM

Part Number: MSP430FR4133
Other Parts Discussed in Thread: HDC2010EVM, ENERGIA, UNIFLASH

I am trying to get the MSP430 launchpad to read from my HDC2010EVM sensor. I have found the resources online with the example code, but I am having difficulty on writing to the pins on the LCD screen. 

I downloaded the example Arduino code to load onto the board. However, I do not see anything showing up on my board at all. I have made sure to set MSP430FR133 as the board in Energia. Is the humidity output supposed to show on the LCD screen or do I need to program it differently?  Also, I am concerned that I may have fried the MSP430 chip- is there a way to check if that device is still working?

Upon reading the MSP430 datasheet, I found that pins 4, 5, 25-64 relate to the LCD pins. However, when looking in the Code Composer code, I see the following lines:

 

#define pos1 4   /* Digit A1 - L4  */

#define pos2 6   /* Digit A2 - L6  */

#define pos3 8   /* Digit A3 - L8  */

#define pos4 10  /* Digit A4 - L10 */

#define pos5 2   /* Digit A5 - L2  */

#define pos6 18  /* Digit A6 - L18 */

 

May you help clarify how I may program the LCD display in the Arduino?

**Attention** This is a public forum