Hello Support member
There is the following description in SLAA666A.(In P3)
3 Addition of RTCLOCK Feature
In the MSP430F67xxA devices, a RTCLOCK feature has been added to reduce the amount of reconfigurations that are necessary after a reset.
SLAU208Q has the following description.(Fig 24-7)
(1) This bit is implemented in only the F677xA, F673xA, and F672xA devices. For other devices, this bit is reserved and always reads as 0.
Q1.
MSP430F6747A does not have a RTCLOCK bit (RTCLOCK feature).
Is this understanding correct?
Best Regards,